Faults and Warning Messages
Jump to a section on this page:
A warning, generally a notification, that is not critical and does not require the machine to immediately shut off. A fault, generally a notification, is a critical system failure that stops machine operation. The severity of the fault depends on which system-stop mechanism is used.
Faults and warnings follow the same pattern and are identified by a four digit code:
G G X X
where GG is a two digit group code and XX is a two digit ID. All faults and warnings are grouped together to easily identify the part of the system having trouble.
| Group | Group # |
|---|---|
| 10 | System |
| 11 | File |
| 15 | Hardware |
| 20 | Power |
| 25 | Temperature |
| 30 | Software |
| 4# | Feedback (# indicates the feedback number) |
| 50 | Motor |
| 55 | Wake and Shake |
| 60 | Motion |
| 70 | Fieldbus |
| 90 | Safety |
Retrieving Fault and Warning Information
Faults are retrieved on a per-axis basis with: AXIS#.FAULTS, where # is the axis number. Similarly, retrieve per-axis warnings with AXIS#.WARNINGS.
DRV.FAULTS returns faults across all axes, with the format X-#### where X is the axis number and #### is the four digit fault code. DRV.WARNING provides warnings across all axes with a similar format.
Feedback faults are reported with axis faults if the feedback is configured as a feedback source for the axis (e.g. AXIS#.IL.FBSOURCE, AXIS#.VL.FBSOURCE , AXIS#.PL.FBSOURCE ). If a feedback is not a feedback source for an axis, its faults are read with FB#.FAULTS where # is the feedback number.
Clearing Faults and Warnings
Once fault conditions are corrected, clear faults on an axis using AXIS#.CLRFAULTS . To clear faults on all axes with a single command, use DRV.CLRFAULTS .
The action table can also be used to clear faults. Action task 12: Clear Faults can be configured to trigger on edge conditions of the action sources. The action task ID selects the axis on which to clear faults.
The hardware enable input can also be used to clear faults. If AXIS#.HWEN.MODE is 0, faults for the axis are cleared on the rising edge of the hardware enable signal.
Fault History
Faults are logged to flash memory for convenience and debugging. To retrieve the last 50 faults with timestamps, use the keyword DRV.FAULTHIST.
To retrieve a more extensive history of faults, use DRV.FAULTHIST/all.
Fault Reaction
The drive’s reaction to a fault is determined by the nature and severity of the fault and the ability of the drive to control motion to zero speed. There are three supported fault reactions:
- Perform a controlled stop to decelerate to zero speed, using the controlled stop configuration for the axis. See Controlled Stop.
- Perform dynamic braking to decelerate the axis to zero speed. See Dynamic Braking.
- Disable the power stage for the axis that allows the connected motor to coast to zero speed.
Fault Table
A list of all possible faults and warnings can be found by using DRV.FAULTLIST.
|
Fault |
Description |
Cause |
Remedy |
Reaction |
|---|---|---|---|---|
|
Firmware and FPGA versions are not compatible. |
The FPGA version does not match the firmware FPGA version constants. |
Load the FPGA version that is compatible with the firmware. |
Disable power stage |
|
|
Power Board type mismatch detected. |
Power board image does not match what operational firmware expected. |
Contact Customer Support to update the drive. |
Disable power stage |
|
|
Power Board Communication fault |
Communications with the Power Board failed. |
Issue AXIS#.CLRFAULTS . If issue persists, contact Technical Support. |
Disable power stage |
|
|
Power Board FPGA not configured. |
Communications with the Power Board failed. |
Issue AXIS#.CLRFAULTS . If issue persists, contact Technical Support. |
Disable power stage |
|
|
Failed to initialize the system. |
Failure in primary module during software start-up. |
Contact Customer Support. |
Disable power stage |
|
|
Unrecognized FPGA fault |
Failure within the FPGA Module. FPGA reported unrecognized fault. |
Issue AXIS#.CLRFAULTS . If problem persists, contact Customer Support. |
Disable power stage |
|
|
FPGA cyclic read fault |
Detected a timing issue between the firmware and FPGA. |
Power cycle the drive. If the fault occurs again, contact Customer Support. |
Disable power stage |
|
|
A Factory MechaWare model failed to load. |
Failed to read the control loop model from flash. |
Power cycle the drive. If the fault occurs again, contact Customer Support. |
Disable power stage |
|
|
A User MechaWare model failed to load. |
Failed to read the user control loop model file from flash. |
Power cycle the drive. If the fault occurs again, contact Customer Support. |
Disable power stage |
|
|
Axis internal |
The firmware detected it was in an unexpected condition. |
Issue AXIS#.CLRFAULTS . If problem persists, contact Customer Support. |
Disable power stage |
|
|
Controlled stop failed |
The deceleration ramp of a controlled stop could not be started. The axis immediately disabled instead. |
Issue AXIS#.CLRFAULTS . If problem persists, contact Customer Support. |
Disable power stage |
|
|
Drive in Fallback after Crash |
The drive has rebooted into Fallback firmware after a crash. |
Contact Customer Support. |
Disable power stage |
|
|
NV Memory Data (might occur when downloading firmware) |
Inconsistency between the non-volatile (NV) parameter definitions and the parameter data stored in NV memory. The fault occurs on startup after downloading firmware. It may happen when upgrading or downgrading firmware versions. |
Compare NV parameters between the original and downloaded versions. Reapply parameter settings that changed. Save NV parameters. Power cycle the drive. |
Disable power stage |
|
|
Flash directory error |
File system in unexpected state. |
Download latest firmware. If problems persist, contact Customer Support |
Disable power stage |
|
|
Identity Read failed |
EDS information on the drive is not in expected format. |
Contact Customer Support |
Disable power stage |
|
|
Invalid MAC Address |
The MAC Address stored in the EDS on the drive is invalid. |
Contact Customer Support |
Disable power stage |
|
|
Power Board factory settings file read failed. |
Power Board settings unable to be retrieved. |
Contact Customer Support |
Disable power stage |
|
|
Power Board update settings file read failed. |
Power Board settings unable to be loaded. |
Contact Customer Support |
Disable power stage |
|
|
Failure reading Control Board FPGA EDS file. |
Control Board configuration settings unable to be loaded. |
Contact Customer Support |
Disable power stage |
|
|
Power Board Resident FPGA not valid. |
Power Board Resident FPGA not valid. |
Update to latest firmware. If problem persists, contact Customer Support. |
Disable power stage |
|
|
Power Board Operational FPGA not valid. |
Power Board Operational FPGA not valid. |
Download latest firmware. If problem persists, contact Customer Support. |
Disable power stage |
|
|
Failure reading Power Board FPGA EDS. |
Failure reading Power Board FPGA EDS. |
Contact Customer Support |
Disable power stage |
|
|
Vbus read is out of thresholds. |
Hardware problem in bus measurement. |
Troubleshoot and repair hardware problem. |
Disable power stage |
|
|
Drive Foldback |
Maximum drive power has been exceeded. The power has been limited to protect the drive. |
Motion requires too much power. Change profile to reduce load. |
Controlled stop |
|
|
Output over current |
Current exceeds drive peak. |
Check for short or feedback faults. |
Disable power stage |
|
|
Current sensor short circuit |
|
|
Disable power stage |
|
|
Iu current offset fault |
Hardware failure detected. |
Disable power stage |
||
|
Iv current offset fault |
Hardware failure detected. |
Disable power stage |
||
|
Bus over voltage |
Bus voltage too high. Usually this problem is load related. |
Reduce load or change motion profile. Check system regen capacity and add capacity, if needed. Check mains voltage. |
Disable power stage |
|
|
Bus under voltage. Warning issued prior to fault. |
Bus voltage below VBUS.UVFTHRESH and the axis was enabled, or bus voltage was below VBUS.INRUSHOFF and the axis was enabled. |
Check mains voltage. |
Controlled stop |
|
|
Bus capacitor overloaded |
Single phase AC input on a drive only rated for three-phase input or excessive single-phase power load. |
Check mains voltage. |
Disable power stage |
|
|
Regen near capacity, could not prevent over voltage. |
An F2006 Bus Over Voltage has occurred while the regen resistor was at or above 75% of its dissipation capacity. |
Increase the size of regen resistor to be able to dissipate more power. |
Disable power stage |
|
|
Regen over power |
Too much power stored in regen resistor. |
Get a larger regen resistor or use DC bus sharing to dissipate power. |
Disable power stage |
|
|
Voltage exceeds motor's rating. |
Drive bus voltage exceeds the motor’s defined voltage rating. |
Make sure that the motor fits the driving rating. |
Disable power stage |
|
|
Power Stage fault |
Power Stage fault |
Clear faults. If problem persists, contact Customer Support. |
Disable power stage |
|
|
Regen short circuit |
Regen resistor short circuit. |
Regen IGBT short circuit. Contact Technical Support. |
Disable power stage |
|
|
AC input phase loss |
Phase loss was detected on three phase AC mains while the drive was enabled. |
Controlled stop |
||
|
Bus over voltage FPGA. |
Bus over voltage hard fault. |
Check mains voltage and check system brake capacity. |
Disable power stage |
|
|
Gate supply under voltage. |
Gate Supply under voltage. |
Check wiring. If problems persist, contact Customer Support. |
Disable power stage |
|
|
Motor Foldback |
Maximum motor power has been exceeded; the power has been limited to protect the motor. |
Motion is requiring too much power. Change move profile to reduce load on motor. Check for load jamming or sticking. Check that current limits are set correctly. |
Controlled stop |
|
|
Broken wire connection to motor. |
At least one of the motor phases are not connected to the drive. For this fault detection to properly work, motor parameters must be set correctly. |
Fix wire connections to the motor. If motor parameters are not set automatically, check motor parameters. |
Disable power stage |
|
|
AC input power loss |
Power loss was detected on AC mains while the drive was enabled. |
Check mains input. If using DC mains, set VBUS.DCOPERATION to 1. |
Controlled stop |
|
|
Initial DC bus above regen threshold. |
An attempt to enable the axis fails due to the DC bus voltage being charged to a steady state voltage greater than the operating threshold of the regen circuits. |
Disable axis |
||
|
Control over temperature |
High temperature limit measured on control circuit. |
Check cabinet ventilation system and ambient temperature. Check fan operation. Check DRV.TEMP to determine whether the temperature measurement is unreasonable or stuck at a high value. |
Disable power stage |
|
|
Power board over temperature |
High temperature limit measured on power board circuit. |
Check cabinet ventilation system and ambient temperature. Check fan operation. Check AXIS1.TEMP and AXIS2,TEMP to determine whether the temperature measurement is unreasonable or stuck at a high value. For more information see: AXIS#.TEMP. |
Disable power stage |
|
|
Control under temperature sensor |
Low temperature limit reached. |
Check cabinet ventilation system and ambient temperature. Check fan operation. Check DRV.TEMP to determine whether the temperature measurement is unreasonable or stuck at a high value. |
Disable power stage |
|
|
Power board under temperature |
Low temperature limit measured on control circuit. |
Check cabinet ventilation system. |
Disable power stage |
|
|
Regen over temperature. |
High temperature limit measured on regen circuit. |
Check cabinet ventilation system and ambient temperature. Check fan operation. Investigate motion that could cause regen circuit to remove power from high DC bus for an extended time. |
Disable power stage. |
|
|
Regen under temperature. |
Low temperature limit measured on regen circuit. |
Check cabinet ventilation system and ambient temperature |
Disable power stage. |
|
|
Issued command timed out. |
Processing a command took longer than the command timeout (10-60 sec depending on the command). |
Try reducing the CPU load of the drive by deactivating unused features or changing the fieldbus cycle time. |
Controlled stop |
|
|
Failed to default parameters. |
Drive parameters could not be reset to default because an axis was enabled. |
Disable all axes. |
Disable power stage |
|
|
Internal firmware error. |
A problem with an internal calculation or data check is preventing the drive from operating correctly. |
|
Disable power stage |
|
|
Operation in Position Mode with Halls Only feedback not allowed. |
Operation in Position Mode with Halls Only feedback not allowed. |
Set your drive’s mode of operation to velocity or torque when using a Halls Only feedback. |
Disable |
|
|
Thread watchdog |
Unresponsive firmware thread. |
Clear faults. If problem persists, contact Customer Support. |
Controlled stop |
|
|
Action Table fault |
This fault is triggered by an action in the action table (when Task = “24 – Fault Axis”). |
Investigate condition that caused fault to trigger. To disable, deactivate the action task that is set to trigger this fault. |
Controlled stop |
|
|
16kHz loop timing above threshold. |
The 16kHz loop took longer than 75% of the total period to complete, likely meaning the drive processor is overloaded. See DRV.CPUPERCENT to monitor processor load. |
Disable user MechaWare models and clear the action table to reduce the processor load, or change DRV.FAULT3008.ACTION to 1 to ignore this condition.
|
Disable power stage |
|
|
MechaWare Model failed to connect Analog Input. |
A MechaWare model contains an Analog Input block with an invalid Analog Input number. |
Fix Analog Input blocks to have valid Analog Input numbers. |
Disable power stage |
|
|
MechaWare Model failed to connect Analog Output. |
A MechaWare model contains an Analog Output block with an invalid Analog Output number. |
Fix Analog Output blocks to have valid Analog Output numbers. |
Disable power stage |
|
|
MechaWare Models are missing Motor Torque block. |
Across all active MechaWare models, there is no Torque Output for all axes. |
|
Disable power stage |
|
|
EEO Faulted. |
EEO is not working due to an error [EEO#.STATUS is 11 (Faulted)]. |
If the Output - Encoder Emulation is using an SFA, make sure the SFA is connected correctly. If the axis is not supposed to be faulted when the EEO is not working, change the configuration in EEO#.FAULTAXIS. |
Controlled stop. |
|
|
Feedback Parity fault |
Feedback Parity fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Overrun fault |
Feedback Overrun fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Framing fault |
Feedback Framing fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback CRC fault |
Feedback CRC fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Communication Timeout fault |
Feedback Communication Timeout fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Initialization Sequence fault |
Feedback Initialization Sequence fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Temperature fault |
Feedback Temperature fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Battery fault |
Feedback battery fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Sensor fault |
Feedback Sensor fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Unique Fault 0 |
Feedback Device-Unique Fault 0 |
Dynamic braking |
||
|
Feedback Device -Unique Fault 1 |
Feedback Device-Unique Fault 1 |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Analog Signal fault |
Feedback Analog Signal fault |
Check feedback settings. If problem persists, Contact Customer Support. |
Dynamic braking |
|
|
Feedback Broken Wire fault |
Feedback broken wire |
Check feedback wiring. |
Dynamic braking |
|
|
Feedback Power Supply fault |
Feedback power supply fault |
Check feedback wiring. |
Dynamic braking |
|
|
Feedback, Illegal Hall State (111 or 000) |
Feedback, Illegal Hall State (111 or 000) |
Check Hall wiring. |
Dynamic braking |
|
|
Failed to set feedback type. |
Failed to set feedback type. |
Check feedback settings and wiring. |
Dynamic braking |
|
|
Failed to read motor parameters from feedback device. |
Motor does not have motor feedback memory or the motor feedback memory is not programmed properly so the parameters cannot be read. |
Try to read parameters again by clicking the Disable and Clear Faults button or by issuing the AXIS#.CLRFAULTS command. If this is not successful, then set AXIS#.MOTOR.AUTOSET to 0 (off) and program the parameters using the setup wizard or manually set up the parameters. If the motor has motor memory (BiSS Analog, EnDat, and SFD motors have motor memory), return the motor to have the memory programmed. |
Dynamic braking |
|
|
SFA communication fault |
Communication error between the SFA and the drive. |
Check cabling between the SFA and the drive. |
Dynamic braking |
|
|
SFA over current |
Feedback power supply over current. |
Check for short-circuit in the cable between the SFA and the drive. |
Dynamic braking |
|
|
SFA under voltage |
High wire resistance or short on cable between SFA and drive. |
Check for loose wiring between the SFA and the drive. |
Dynamic braking |
|
|
Feedback: safety fault |
Feedback safety system has faulted. |
Check for damaged encoder. Replace if problem persists. |
Dynamic braking |
|
|
Feedback: Watchdog fault |
Feedback subsystem stopped responding. |
Internal system fault. Report failure to Kollmorgen. |
Dynamic braking |
|
|
Unrecognized feedback fault. |
FPGA reported unrecognized fault. |
Issue AXIS#.CLRFAULTS . If problem persists, contact Customer Support. |
Dynamic braking |
|
|
SFA Resident FPGA not valid. |
Check if FPGA file on SFA failed. |
Restart drive and reselect SFA feedback type. Update to latest SFA firmware. If problem persists, contact Customer Support. |
Disable power stage |
|
|
SFA Operational FPGA not valid. |
Check if FPGA file on SFA failed. |
Restart drive and reselect SFA feedback type. Update to latest SFA firmware. If problem persists, contact Customer Support. |
Disable power stage |
|
|
SFA FPGA file read failed. |
FPGA file on SFA could not be read due to communication issue. |
Restart drive and reselect SFA feedback type. Update to latest SFA firmware. If problem persists, contact Customer Support. |
Disable power stage |
|
|
SFA Factory file read failed. |
Configuration file on SFA could not be read due to communication issue. |
Restart drive and reselect SFA feedback type. If problem persists, contact Customer Support. |
Disable power stage |
|
|
Firmware and SFA versions are not compatible. |
The SFA major version does not match the version the firmware expects. |
Disable power stage |
||
|
The feedback position changed while the power was off and Store Multiturn enabled. |
The feedback position changed while the power was off and Store Multiturn enabled. |
|
Disable power stage |
|
|
The Store Multiturn feature requires an absolute device. |
The Store Multiturn feature requires an absolute device. |
|
Disable power stage |
|
|
SFA model does not support feedback type |
There are several different SFA models and each supports a different set of feedback devices. You are using an SFA that does not support the feedback selected with FB#.SELECT.
|
|
Disable power stage |
|
|
Motor overheated. |
Motor overheated. |
Check ambient temperature. Check motor mounting heat sink capability. |
Controlled stop |
|
|
Brake 1 current out of range. |
Brake 1 current out of range detected on drive with pass-thru hardware. Brake 1 current measurement error on drive with SMM hardware. |
Check brake wiring. |
Dynamic braking |
|
|
Brake 2 current out of range. |
Brake 2 current out of range detected on drive with pass-thru hardware. Brake 2 current measurement error on drive with SMM hardware. |
Check brake wiring. |
Dynamic braking |
|
|
Brake applied when it should be released. |
Motor brake closed unexpectedly. |
Check cabling and general functionality. |
Dynamic braking |
|
|
Brake released when it should be applied. |
Brake disengaged unexpectedly. |
Check cabling and general functionality. |
Controlled stop |
|
|
Drive motor parameters setup incomplete. |
Before a motor can be enabled, you must configure a minimum set of parameters. These parameters have not been configured. |
Issue the command AXIS#.SETUPREQLIST to display the list of the parameters you must configure. Configure these parameters manually or automatically. You can manually configure these parameters in three ways:
|
Disable power stage |
|
|
Temperature sensor detected open circuit. |
Motor thermal sensor measurement indicates expected sensor is not connected. |
Check temperature sensor connection. Verify thermal sensor type (AXIS#.MOTOR.RTYPE) is correct. |
Controlled stop |
|
|
F5011 |
Brake 1 under current. |
Brake 1 current too low on drive with SMM hardware. |
Check brake wiring. |
Dynamic braking |
|
F5012 |
Brake 2 under current. |
Brake 2 current too low on drive with SMM hardware. |
Check brake wiring. |
Dynamic braking |
|
Brake 1 over current. |
Brake 1 current too high on drive with SMM hardware. |
Check brake wiring. |
Dynamic braking |
|
|
Brake 2 over current. |
Brake 2 current too high on drive with SMM hardware. |
Check brake wiring. |
Dynamic braking |
|
|
AXIS#.IL.FBSOURCE has unidentified feedback selected. |
The type of the feedback referenced by AXIS#.IL.FBSOURCE was not identified successfully. |
Check the connection for the feedback referenced by AXIS#.IL.FBSOURCE. Check FB#.SELECT is correct for the feedback. |
Disable power stage |
|
|
AXIS#.VL.FBSOURCE has unidentified feedback selected. |
The type of the feedback referenced by AXIS#.VL.FBSOURCE was not identified successfully. |
Check the connection for the feedback referenced by AXIS#.VL.FBSOURCE . Check FB#.SELECT is correct for the feedback. |
Disable power stage |
|
|
AXIS#.PL.FBSOURCE has unidentified feedback selected. |
The type of the feedback referenced by AXIS#.PL.FBSOURCE was not identified successfully. |
Check the connection for the feedback referenced by AXIS#.PL.FBSOURCE . Check FB#.SELECT is correct for the feedback. |
Disable power stage |
|
|
Sensorless control only available in velocity mode. |
Axis whose op mode is not velocity is configured for sensorless control. |
Set AXIS#.OPMODE = 1 (Velocity Mode). |
Disable power stage |
|
|
Wake and Shake - Insufficient movement |
There was less movement than defined by AXIS#.WS.DISTMIN |
Increase AXIS#.WS.IMAX and/or AXIS#.WS.T . Or try using AXIS#.WS.MODE 1 or 2. |
Disable power stage |
|
|
Wake and Shake - Excess movement |
AXIS#.WS.DISTMAX has been exceeded in AXIS#.WS.MODE 0. Or more than 360 degrees was traveled in AXIS#.WS.MODE 2. |
Increase AXIS#.WS.DISTMAX value or reduce AXIS#.WS.IMAX or AXIS#.WS.T . Wake and Shake is not supported for vertical/overhung loads. |
Disable power stage |
|
|
Wake and Shake - Fine-Coarse delta too large |
The angle difference between the coarse and fine calculation was larger than 72 deg. |
Modify AXIS#.WS.IMAX or AXIS#.WS.T and try again. |
Disable power stage |
|
|
Wake and Shake - Over speed |
AXIS#.WS.VTHRESH was exceeded. |
Increase AXIS#.WS.VTHRESH value or reduce AXIS#.WS.IMAX or AXIS#.WS.T . |
Disable power stage |
|
|
Wake and Shake - Loop angle delta too large |
The angle between complete loops was larger than 72 deg. |
Modify AXIS#.WS.IMAX or AXIS#.WS.T and try again. |
Disable power stage |
|
|
Wake and Shake - Commutation not initialized |
The motor requires the commutation initialization (there are no encoder commutation tracks, Hall sensors, etc.) and no successful Wake and Shake sequence has been performed. |
Clear any faults, activate the Wake and Shake procedure (AXIS#.WS.ARM ), and enable the drive. |
Disable power stage |
|
|
Wake and Shake - Motor U phase missing |
No current was detected in the motor's U phase during Wake and Shake initialization (Mode 0 only). |
Check the motor connections and AXIS#.WS.IMAX (very low current may produce this error). |
Disable power stage |
|
|
Wake and Shake - Motor V phase missing |
No current was detected in the motor's V phase during Wake and Shake initialization (Mode 0 only). |
Check the motor connections and AXIS#.WS.IMAX (very low current may produce this error). |
Disable power stage |
|
|
Wake and Shake - Motor W phase missing |
No current was detected in the motor's W phase during Wake and Shake initialization (Mode 0 only). |
Check the motor connections and AXIS#.WS.IMAX (very low current may produce this error). |
Disable power stage |
|
|
Wake and Shake - validating positive movement failed |
After applying a positive current, motor moved in the wrong direction. |
Check motor phase wiring and motor encoder wiring is correct. |
Disable power stage |
|
|
Wake and Shake - validating negative movement failed |
After applying a negative current, motor moved in the wrong direction. |
Check motor phase wiring and motor encoder wiring is correct. |
Disable power stage |
|
|
Wake and Shake - validating comm. angle timed out |
During one of the Wake and Shake validation stages, the drive stopped responding to commands. |
Contact Customer Support. |
Disable power stage |
|
|
Wake and Shake - validating comm. angle moved too far - bad comm angle |
After applying a current, the motor moved too far (>15 electrical degrees). |
This indicates a poor motor phase angle was found by Wake and Shake. Revise Wake and Shake parameters and re-run Wake and Shake. |
Disable power stage |
|
|
Wake and Shake - validating comm. angle required more than AXIS#.MOTOR.ICONT |
A current larger than AXIS#.MOTOR.ICONT was used to excite the motor. |
This indicates one of the following:
|
Disable power stage |
|
|
Wake and Shake - limit switch hit |
A digital input configured as a limit switch through the action table has triggered or the position feedback is outside software position limits. |
Move the load away from the limits. |
Disable power stage |
|
|
Wake and Shake is not compatible with Gantry configurations. |
Wake and Shake was started with an axis configured as a Gantry. |
Make sure no axis has Gantry as its Command Source. |
Disable power stage |
|
|
Wake and Shake is not supported when AXIS#.IL.OFFSET is non-zero |
Wake and Shake was started with AXIS#.IL.OFFSET set to a non-zero value. |
Set AXIS#.IL.OFFSET to zero until commutation has been established. |
Disable power stage |
|
|
Over speed |
Motor exceeded AXIS#.VL.THRESH . |
Increase AXIS#.VL.THRESH or lower velocity command. |
Dynamic braking |
|
|
Following error magnitude fault |
Motor did not follow command values. Motor exceeded maximum allowed position following error (user). |
Check feedback commutation setup and tuning parameters. |
Controlled stop |
|
|
Invalid commutation detected - motor accelerating in the wrong direction. Motor phase may be incorrect. |
The velocity of the motor exceeded AXIS#.WS.CHECKV and the sign of the current was not equal to the sign of motor acceleration or the sign of motor velocity for a period of time larger than AXIS#.WS.CHECKT. |
|
Dynamic braking |
|
|
Instability during autotune |
Drive current (AXIS#.IL.CMD ) or velocity feedback (AXIS#.VL.FB ) exceeds allowable limit (AXIS#.BODE.IFLIMIT or AXIS#.BODE.VFLIMIT). This fault only occurs in AXIS#.BODE.MODE 5. This fault often occurs when complex mechanics, belts, and compliant loads are present. |
Change AXIS#.BODE.MODE if appropriate. If AXIS#.BODE.MODE 5 is appropriate and the fault occurs at the end of an Autotuning, then the motor is not robustly stable. You can manually adjust Autotuner settings. Manual tuning may be required to make the motor stable. |
Controlled stop |
|
|
Target position was overshot due to invalid motion task activation. |
The drive cannot decelerate from its current speed to reach the end point of the second Motion Task without moving past it. Increase the deceleration rate in the move or trigger the move earlier. |
Change Motion Task profile and clear fault with AXIS#.CLRFAULTS . Or change the value of AXIS#.FAULT6004.ACTION . |
Default is 0: Disable Amplifier. |
|
|
Emergency timeout occurred. |
Motor did not stop in the timeout defined in AXIS#.DISTO . |
Change timeout value, change stop parameters and improve tuning. |
Disable power stage |
|
|
Current home mode requires AXIS#.HOME.IPEAK to be set. |
Some homing modes require AXIS#.HOME.IPEAK to be a non-zero value. |
Set AXIS#.HOME.IPEAK to a non-zero value or use a different homing mode (AXIS#.HOME.MODE). |
Disable power stage |
|
|
Gantry master faulted. |
The master axis of the gantry has faulted causing the slave to fault. |
DRV.CLRFAULTS to clear both axes’ faults. |
None |
|
|
Gantry slave faulted. |
The slave axis of the gantry has faulted causing the master to fault. |
DRV.CLRFAULTS to clear both axes’ faults. |
None |
|
|
Sensorless control fault. |
Sensorless observer unable to track motor angle. |
Check that sensorless tuning parameters are correct. Investigate disturbances to axis motion. |
Dynamic brake |
|
|
Gearing feedback source is invalid. |
The feedback selected as the gearing source is uninitialized or assigned to the same feedback being used as the commutation, velocity, or position feedback source. |
Verify AXIS#.GEAR.FBSOURCE is not 0 and does not match the feedback being used for AXIS#.IL.FBSOURCE, AXIS#.VL.FBSOURCE , AXIS#.PL.FBSOURCE . |
Controlled stop |
|
|
Gantry position error fault |
GANTRY.PL.ERR exceeded GANTRY.PL.ERRWTHRESH. |
Increase warning threshold, fix mechanical linkage, improve tuning or remove disturbances. |
Disable power stage |
|
|
Fieldbus communication lost.
Fieldbus: All but Modbus.
EtherNet/IP Explanation: EtherNet/IP connection timed out |
All fieldbus communication was lost.
EtherNet/IP Potential Causes: Cable disconnection or network issues between PLC and drive |
Check fieldbus connections, settings, and control unit.
EtherNet/IP Remedies: Ensure the network cable is connected to the fieldbus port on the drive and there is nothing preventing passage of network packets between the PLC and the drive |
Controlled stop |
|
|
Fieldbus sync frames lost.
Fieldbus: EtherCAT |
The fieldbus lost synchronization. |
Check fieldbus connection or the settings of your EtherCAT or CANopen master. |
Controlled stop |
|
|
Fieldbus Heartbeat lost
Fieldbus: EtherCAT |
Heartbeat lost. |
Check CANopen cabling. Reduce bus load or increase the heartbeat update time. |
Controlled stop |
|
|
PLL failed to lock.
Fieldbus: All but Modbus.
EtherNet/IP Explanation: PLL took too long to lock |
Fieldbus PLL failed to lock.
EtherNet/IP Potential Causes: A connection was made, causing the PLL to try to lock, but a lost or inconsistent update rate caused the lock to fail
|
Check fieldbus wiring and settings. Remedies: Check that the connection is consistent between drive and PLC.
|
Controlled stop |
|
|
PLL lost lock.
Fieldbus: All with PLL (comes with FPGA).
EtherNet/IP Explanation: PLL lost lock |
Fieldbus PLL lost lock.
EtherNet/IP Potential Causes: |
Check fieldbus wiring and settings
EtherNet/IP Remedies: Check that connection is consistent between drive and PLC
|
Controlled stop |
|
|
Fieldbus cyclic setpoints missing.
Fieldbus: EtherCAT, EtherNet/IP
EtherNet/IP Explanation: Missed too many packets from the PLC |
Fieldbus communication interrupted.
EtherNet/IP Potential Causes: Drive missed three or more packets with streaming active, or twelve or more packets in a row without streaming active |
Check fieldbus wiring and settings.
EtherNet/IP Remedies:
|
Controlled stop |
|
|
Fieldbus initialization failed.
Fieldbus: All but Modbus
EtherNet/IP drives: Incompatible internal EtherNet/IP Adapter firmware version installed.
EtherNet/IP Explanation: EtherNet/IP fieldbus initialization failed |
CAN-wiring might be wrong or internal failure.
EtherNet/IP Potential Causes: Bad internal EtherNet/IP Adapter firmware or other internal issue. |
Check CAN-wiring and termination or contact Customer Support.
For EtherNet/IP drives, install the correct internal EtherNet/IP Adapter firmware version for the installed drive firmware version. The installed internal EtherNet/IP Adapter firmware version can be viewed with the EIP.INFO keyword. |
Controlled stop |
|
|
Sign of life error counter exceeded threshold.
Fieldbus: PROFINET |
PROFINET synchronization issues. The PLC sign of life counter is not increasing by 1 each cycle, indicating missed samples. |
Check Ethernet cables, PLC load, network issues. |
Controlled stop |
|
|
Telegram configuration invalid.
Fieldbus: PROFINET |
The free mapping telegram or supplemental telegram is used and is configured incorrectly. Verify no duplicate signals are mapped and 32-bit signals are mapped correctly (two 16-bit slots used). |
Correct the telegram configuration. |
Controlled stop |
|
|
Fieldbus shutdown.
Fieldbus: EtherNet/IP, PROFINET
EtherNet/IP Explanation: EtherNet/IP application shutdown unexpectedly |
Internal drive firmware error.
EtherNet/IP Potential Causes: Bad internal EtherNet/IP Adapter firmware |
Reboot the drive. If problem persists, contact Customer Support.
EtherNet/IP Remedies: Check internal EtherNet/IP Adapter firmware is correct using EIP.INFO. |
Controlled stop |
|
|
EtherCAT synchronization error
Fieldbus: EtherCAT |
The error counter limit 10F1h sub 2 (ECAT.MAXSYNCERROR) was exceeded by one of the error counters defined by object 1C33h sub 11 or 13. It is possible, but not recommended, to switch the supervision off by setting a value of 0. |
Either change the input shift via object 1C33h sub 3 (ECAT.INPUTSHIFTU) or try to minimize the EtherCAT master’s jitter. |
Controlled stop |
|
|
Fieldbus cyclic setpoint buffer overload
Fieldbus: EtherNet/IP
EtherNet/IP Description: The interpolator queue was full but still received another point |
Update rate mismatch that results in receiving more points than are being consumed |
Check that the PLC update rate (Motion Group) is not faster than Stream Period
|
Controlled stop |
|
|
Fieldbus velocity command too low. |
Fieldbus commanded a velocity lower than the minimum limit. |
Increase fieldbus velocity command or change AXIS#.FAULT7015.ACTION to allow motion to continue. If motion continues, the velocity will be clamped at AXIS#.VL.LIMITN. |
See AXIS#.FAULT7015.ACTION Default is 1: Ignore (Fault will not be reported). |
|
|
Fieldbus velocity command too high. |
Fieldbus commanded a velocity higher than the maximum limit.
|
Reduce fieldbus commanded velocity or change AXIS#.FAULT7016.ACTION to allow motion to continue. If motion continues, the velocity will be clamped at AXIS#.VL.LIMITP. |
See AXIS#.FAULT7016.ACTION . Default is 1: Ignore. (Fault will not be reported). |
|
|
Fieldbus position setpoints took too long to be updated.
Fieldbus: EtherNet/IP |
Drive received at least three fieldbus commands in a row that arrived later than expected. This fault can also be triggered by commands with timestamps that are older than or the same as the previous command received. |
|
Controlled stop |
|
|
Modbus watchdog timer expired
Fieldbus: Modbus |
The Ethernet connection from the HMI to the AKD2G was broken unexpectedly. Possible causes are the cable is disconnected or broken or power is lost to the HMI or any Ethernet switches. See MODBUS.WATCHDOG. |
Fix the cable or fix the HMI power to switches. |
Controlled stop |
|
|
Modbus keepalive detected connection loss
Fieldbus: Modbus |
The Ethernet connection from the HMI to the AKD2G was broken unexpectedly. Possible causes are the cable is disconnected or broken or power is lost to the HMI or any Ethernet switches. See MODBUS.KEEPALIVE. |
Fix the cable or fix the HMI power to switches. |
Controlled stop |
|
|
Safe torque off. |
Safe torque off function has been triggered. F9000 is only generated if AXIS#.SAFE.STO.REPORTFAULT is 1. |
Reapply supply voltage to STO if safe to do so. |
Disable power stage |
|
|
SMM communication failed. |
Safe Motion Module not communicating as expected. |
Contact Customer Support. |
Disable power stage |
|
|
Incorrect safety card detected. |
Physical SMM module does not match the expected module. |
Contact Customer Support. |
Disable power stage |
|
|
Safe torque off digital and analog lines don't match. |
Hardware fault on the power board . |
Restart Drive. If issue persists, contact technical support. |
Controlled stop |
|
|
STO Simultaneity |
The two STO inputs did not change state within 100 ms of each other. |
Check wiring and safety apparatus |
Controlled stop |
|
|
SMM in failed state. |
SMM detected a safety I/O failure and faulted. This can be caused by: digital I/O pulse failed, STO pulse failed, encoder position failure, or serial communication failed. |
Determine cause and replace necessary hardware if issue reoccurs. |
Controlled stop |
|
|
Safe brake parameters inconsistent. |
The safe parameter, AXIS#.SAFEPARAM.SBC.BRAKE#ATTACHED, indicate a brake is attached, but non-safe brake keywords, AXIS#.MOTOR.BRAKE , BRAKE#.AXIS, do not and drive was enabled. |
From the safety parameter screen in WorkBench under safe brake control (SBC), verify the SBC Brake parameters agree with the drive related parameters that a brake is configured or not.
The keywords AXIS#.MOTOR.BRAKE , BRAKE#.AXIS, and safe brake control configuration (SBC) all must agree with each other. For example, if no brake is present AXIS#.MOTOR.BRAKE should be 0 and safe parameters for SBC should indicate ‘Not Configured’. If brake is present, AXIS#.MOTOR.BRAKE should be 1, BRAKE#.AXIS should be assigned to proper axis, and safe parameters for SBC should be set to ‘Configured…’.
AXIS#.SAFEPARAM.SBC.BRAKE1ATTACHED and AXIS#.SAFEPARAM.SBC.BRAKE2ATTACHED can be verified for the currently active safe parameters. |
Disable power stage |
Warning Table
A list of all possible warnings can be found by using DRV.WARNINGLIST.
| Warning | Description | Cause | Remedy |
|---|---|---|---|
| W1000 | Fan stalled. | Fan speed is too slow. | Power Cycle drive. If problem persists, contact Customer Support. |
| W1001 | Sync timer PLL | FPGA Synchronization is off. | Update to latest firmware. If problem persists, contact Customer Support. |
| W1500 | Drive in fallback. | The regular drive firmware has experienced a fatal issue and is running in recovery mode. | Contact Kollmorgen Customer Support |
| W1501 | Test control board FPGA loaded. | A test FPGA image is on the control board. | Load official release firmware. |
| W1502 | Test power FPGA loaded. | A test FPGA image is on the power board. | Load official release firmware. |
| W1503 | Test firmware loaded. | Non-release test firmware detected. | Load official release firmware. |
| W1504 | Incorrect EDS parameter definitions. | An electronic data sheet file containing drive identity information has inconsistent parameter definitions. The parameters are set to default values that allow the drive to operate. This condition is rare, but may occur after a firmware udpate. |
|
| W2001 | Drive foldback imminent! Reduce Load. | Current command is high enough to trip Drive Foldback threshold. | Decrease current command by softening tuning gains or a less aggressive motion trajectory. If problem persists, application may require a drive with larger power rating. |
| W2002 | Motor foldback imminent! Reduce Load. | Current command is high enough to trip Motor Foldback threshold. | Decrease current command by softening tuning gains or a less aggressive motion trajectory. If problem persists, application may require a motor with larger power rating. |
| W2003 | Motor I2t load! Reduce load. | Current command is high enough to trip Motor I²t threshold. | Decrease current command by softening tuning gains or a less aggressive motion trajectory. If problem persists, application may require a motor with larger power rating. |
| W2006 | Bus over voltage | Line voltage spiked above VBUS.OVWTHRESH, or motor back emf generated voltage above VBUS.OVWTHRESH. | Clear faults. If problem persists, determine source of voltage spike. If problem is power related, power conditioning may be required. If voltage spike is due to motor back-emf, a regen resistor may be required for the application. |
| W2007 | Bus under voltage | Bus voltage dipped below VBUS.UVWTHRESH | Check supply voltage. |
| W2008 | Bus capacitor overloaded | Internal voltage spiked above VBUS.OVWTHRESH or motor back emf generated voltage above VBUS.OVWTHRESH. | Clear faults. If problem persists, determine source of voltage spike. If problem is power related, power conditioning may be required. If voltage spike is due to motor back emf, a regen resistor may be required for the application. |
| W2010 | Regen energy critical | Regen resistor is reaching its capacity. | Decrease aggressiveness of motion profile or use larger size regen resistor. |
| W2011 | No Power on IO 24V rail |
24 volts was not detected on x21 connector.
|
Connect +24V to B3 (24V_I/O) on x21 and GND to B4 (GND_I/O) on x21 and verify wire integrity. |
| W2012 | Initial DC bus is greater than regen threshold | The DC bus voltage is being charged to a steady state voltage greater than the operating threshold of the regen circuits. | W2012 Detailed Troubleshooting Steps |
| W2014 | AC input phase loss |
Occurs when the drive hardware:
|
F2014 Detailed Troubleshooting Steps |
| W2019 | AC input power loss | Power loss was detected on AC mains. | Check mains input. If using DC mains, set VBUS.DCOPERATION to 1. |
| W2500 | Control over temperature | Low temperature limit measured on power board circuit. | Increase air circulation around drive box and check fan operation. |
| W2501 | Power board over temperature | Internal power board temperature is overheating. | Increase air circulation around drive box and check fan operation. |
| W2502 | Control under temperature | Internal control board is getting below specified operating temperature. | Check cabinet ventilation system and ambient temperature. |
| W2503 | Power board under temperature. | Internal power board is getting below specified operating temperature. | Check cabinet ventilation system and ambient temperature. |
| W2504 | Regen over temperature. | Regen circuit temperature is overheating. | Increase air circulation around drive box and check fan operation. Investigate motion that could cause regen circuit to remove power from high DC bus for an extended time. |
| W2505 | Regen under temperature. | Internal regen circuit temperature is getting below specified operating temperature. | Check cabinet ventilation system and ambient temperature. |
| W3001 | Ethernet interface throttled. | Packets are arriving at Ethernet interface faster than the drive can process. | Check devices that could be sending packets to the drive. If possible, move the drive to a different or dedicated LAN. |
| W3007 | Action table error. | The drive encountered an error during execution of an action task. See ACTION.ERRORS / ACTION#.ERROR for more information. | Only trigger actions if their task can be executed. ACTION.ERRORS / ACTION#.ERROR will indicate why the task failed. |
| W3100 | An axis has a duplicate Actual Position Feedback block. | Across all active MechaWare models, there is more than one Actual Position Feedback block for an axis. |
|
| W3101 | An axis has a duplicate AXIS#.PL.CMD block. | Across all active MechaWare models, there is more than one AXIS#.PL.CMD block for an axis. |
|
| W3102 | An axis has a duplicate AXIS#.PL.ERR block. | Across all active MechaWare models, there is more than one AXIS#.PL.ERR block for an axis. |
|
| W3103 | An axis has a duplicate Position Int Out block. | Across all active MechaWare models, there is more than one Position Int Out block for an axis. |
|
| W3104 | An axis has a duplicate AXIS#.VL.CMD block. | Across all active MechaWare models, there is more than one AXIS#.VL.CMD block for an axis. |
|
| W3105 | An axis has a duplicate AXIS#.VL.FB block. | Across all active MechaWare models, there is more than one AXIS#.VL.FB block for an axis. |
|
| W3106 | An axis has a duplicate AXIS#.VL.ERR block. | Across all active MechaWare models, there is more than one AXIS#.VL.ERR block for an axis. |
|
| W3107 | An axis has a duplicate Trajectory VCmd block. | Across all active MechaWare models, there is more than one Trajectory VCmd block for an axis. |
|
| W3108 | An axis has a duplicate AXIS#.IL.FF block. | Across all active MechaWare models, there is more than one AXIS#.IL.FF block for an axis. |
|
| W3109 | An axis has a duplicate OpenLoopFeedback block. | Across all active MechaWare models, there is more than one OpenLoopFeedback block for an axis. |
|
| W3110 | An axis has a duplicate VelocityPIOut block. | Across all active MechaWare models, there is more than one VelocityPIOut block for an axis. |
|
| W3111 | An axis has a duplicate PreBodeExcite block. | Across all active MechaWare models, there is more than one PreBodeExcite block for an axis. |
|
| W3112 | An axis has a duplicate Motor Torque block. | Across all active MechaWare models, there is more than one Motor Torque block for an axis. |
|
| W3113 | A duplicate AnalogOut block exists. | Across all active MechaWare models, there is more than one Analog Out block with the same output number. |
|
| W3114 | A duplicate DigitalOut block exists. | Across all active MechaWare models, there is more than one Digital Out block with the same output number. |
|
| W3115 | A duplicate UserBuffer block exists. | Across all active MechaWare models, there is more than one UserBuffer block with the same output number. |
|
| W3116 | A duplicate Simulated Feedback block exists. | Across all active MechaWare models, there is more than one Simulated Feedback block with the same output number. |
|
| W3117 | An axis is missing its AXIS#.PL.CMD block. | Across all active MechaWare models, an axis is missing its AXIS#.PL.CMD block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3118 | An axis is missing its AXIS#.PL.ERR block. | Across all active MechaWare models, an axis is missing its AXIS#.PL.ERR block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3119 | An axis is missing its Position Int Out block. | Across all active MechaWare models, an axis is missing its Position Int Out block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3120 | An axis is missing its AXIS#.VL.CMD block. | Across all active MechaWare models, an axis is missing its AXIS#.VL.CMD block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3121 | An axis is missing its AXIS#.VL.FB block. | Across all active MechaWare models, an axis is missing its AXIS#.VL.FB block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3122 | An axis is missing its AXIS#.VL.ERR block. | Across all active MechaWare models, an axis is missing its AXIS#.VL.ERR block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3123 | An axis is missing its Trajectory VCmd block. | Across all active MechaWare models, an axis is missing its Trajectory VCmd block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3124 | An axis is missing its AXIS#.IL.FF block. | Across all active MechaWare models, an axis is missing its AXIS#.IL.FF block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3125 | An axis is missing its OpenLoopFeedback block. | Across all active MechaWare models, an axis is missing its OpenLoopFeedback block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3126 | An axis is missing its VelocityPIOut block. | Across all active MechaWare models, an axis is missing its VelocityPIOut block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3127 | An axis is missing its PreBodeExcite block. | Across all active MechaWare models, an axis is missing its PreBodeExcite block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3128 | An axis is missing its Motor Torque block. | Across all active MechaWare models, an axis is missing its Motor Torque block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3129 | An axis is missing its Position Command block. | Across all active MechaWare models, an axis is missing its Position Command block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3130 | An axis is missing its Position Feedback block. | Across all active MechaWare models, an axis is missing its Position Feedback block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3131 | An axis is missing its Velocity Command block. | Across all active MechaWare models, an axis is missing its Velocity Command block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3132 | An axis is missing its Bode Torque block. | Across all of the active MechaWare models, an axis is missing its Bode Torque block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W3133 | An axis is missing its Bode Velocity block. | Across all active MechaWare models, an axis is missing its Bode Velocity block. |
1. Verify correct models are active. 2. Modify user models and add required block for each axis. |
| W4x00 | Feedback Parity warning | Feedback Parity warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x01 | Feedback Overrun warning | Feedback Overrun warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x02 | Feedback Framing warning | Feedback Framing warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x03 | Feedback CRC warning | Feedback CRC warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x04 | Feedback Communication Timeout warning | Feedback Communication Timeout warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x05 | Feedback Initialization Sequence warning | Feedback Initialization Sequence warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x06 | Feedback Temperature warning | Feedback Temperature warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x07 | Feedback Battery warning | Feedback Battery warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x08 | Feedback Sensor warning | Feedback Sensor warning | Check feedback settings. If problem persists, contact Customer Support. |
| W4x09 | Feedback Device-Unique Warning 0 | Feedback Device-Unique Warning 0 | Check feedback settings. If problem persists, contact Customer Support. |
| W4x10 | Feedback Device-Unique Warning 1 | Feedback Device-Unique Warning 1 | Check feedback settings. If problem persists, contact Customer Support. |
| W4x11 | Warning: Gearing feedback source fault | Fault condition was detected on position feedback device referenced by AXIS#.GEAR.FBSOURCE. |
|
| W4x12 | Test SFA FPGA loaded. | A test FPGA image is on the SFA. | Load official release firmware. |
| W4x13 | Feedback hall sequence invalid. | The drive detected a bad hall sequence usually due to incorrect hall wiring. | Physically wire the hall signals correctly or use FB#.HALLMAP.U/FB#.HALLMAP.V/FB#.HALLMAP.W to virtually wire the hall signals correctly. |
| W4x31 | Feedback hall sequence invalid. | The halls on the motor with the specified feedback were detected out of sequence. | Monitor FB#.HALLSTATE (must use FB#.MONITOR* keywords when using an SFA) to determine which hall signal is out of sequence and correct wiring or run the motor setup wizard. In rare instances the halls sensors may have become mispositioned and need repair. |
| W5000 | Motor overheated | Motor overheated | Check ambient temperature and motor mounting heat sink capability. |
| W5007 | Brake override active, but no brake configured. | Brake override is active on an axis that has no brake configured. | The parameter AXIS#.MOTOR.BRAKECONTROL overrides actual brake control of the drive. |
| W5008 | Brake override active | Brake override active | The parameter AXIS#.MOTOR.BRAKECONTROL overrides actual brake control of the drive. |
| W5500 | Wake and Shake - Over speed | AXIS#.WS.VTHRESH was exceeded. | Increase AXIS#.WS.VTHRESH value or reduce AXIS#.WS.IMAX or AXIS#.WS.T . |
| W5515 | Wake and Shake is not compatible with Gantry configurations. | Wake and Shake was armed with an axis configured as a Gantry. | Make sure no axis has Gantry as its Command. |
| W5516 | Wake and Shake is not supported when AXIS#.IL.OFFSET is non-zero. | Wake and Shake was started with AXIS#.IL.OFFSET set to a non-zero value. | Set AXIS#.IL.OFFSET to zero until commutation has been established. |
| W6000 | When a motion task, service motion or homing move is started, the drive checks to see if the motion would exceed the range given by AXIS#.VL.LIMITP and AXIS#.VL.LIMITN. If this range is exceeded, the motion is modified to be within range and this warning is generated. This warning is latched and only cleared if a new motion is commanded or AXIS#.CLRFAULTS is used. This means the last motion started was modified to fit into the velocity limits. | Last motion command exceeds velocity limit. | Starting any new motion or using AXIS#.CLRFAULTS clears the warning. To ensure the warning is not immediately generated again make sure the motion task or service motion target velocity is within the AXIS#.VL.LIMITP and AXIS#.VL.LIMITN range. |
| W6001 | Following error magnitude fault. | Motor did not follow command values. Motor exceeded maximum allowed position following error AXIS#.PL.ERRWTHRESH . | Check feedback commutation setup and tuning parameters. |
| W6002 | Homing is needed. | Attempt to issue motion task before the axis is homed. Axis must be homed before motion task can start. | Change opmode or home axis. |
| W6003 | OPMODE incompatible with CMDSOURCE | This warning is generated when the drive is enabled and the gearing command source is selected at the same time as torque or velocity opmode. | Select a different AXIS#.OPMODE and AXIS#.CMDSOURCE combination. |
| W6004 | Zero velocity when using induction sensorless feedback type in torque mode. | Zero velocity when using induction sensorless feedback type in torque mode. | Check motor wiring and tuning parameters. If problem persists, contact Customer Support. |
| W6005 | Velocity has been limited commutation speed to less than 600Hz to meet ECCN 3A225 requirements. | Motor Velocity has exceeded the allowed commutation speed (599Hz). | Refer to Frequency / Velocity Limitation for Open Loop Motor Control. |
| W6006 | Positive limit switch triggered | A digital input is configured as positive limit switch (DINx.MODE 18) and its state is “off” or a positive software position limit is configured (AXIS#.SWLS.EN) and the actual position AXIS#.PL.FB is greater than the configured limit (see also AXIS#.SWLS.LIMIT#). | Move the load away from the limits. |
| W6007 | Negative limit switch triggered | A digital input is configured as negative limit switch (DINx.MODE 19) and its state is “off” or a negative software position limit is configured (AXIS#.SWLS.EN) and the actual position AXIS#.PL.FB is less than the configured limit (see also AXIS#.SWLS.LIMIT#). | Move the load away from the limits. |
| W6008 | Using derivative of position when using sensorless feedback type in position mode. | Using derivative of position when using sensorless feedback type in position mode. | Sensorless operation is not allowed for Position Mode - change AXIS#.OPMODE to Velocity Mode. |
| W6009 |
Following motion failed, check motion parameters. |
Activation of the motion task failed due to incompatible parameters or motion task does not exist. |
Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. Check following motion task settings and parameters to make sure the values entered will produce a valid motion task. |
| W6010 | Target position crossed due to stop command. | The motion task crosses the target position after triggering an AXIS#.STOP command. This can happen when processing a change on the fly motion task and triggering an AXIS#.STOP command close to the target position of the currently running motion task. | Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. |
| W6011 | Homing index pulse not found. | A homing mode with index detection is activated and index pulse is not detected while moving across the range determined by the hardware limit switches. | Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. |
| W6012 | Homing reference switch not found. | A homing mode with reference switch detection is activated and the reference switch is not detected while moving across the range determined by the hardware limit switches. | Activation of any new motion or use ofAXIS#.CLRFAULTS clears the warning. |
| W6014 |
Motion task activation failed. |
Activation of the motion task failed due to incompatible parameters or motion task does not exist. This warning can appear upon an AXIS#.MT.MOVE command. |
Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task. |
| W6015 | Homing procedure failed. | Homing error observed during the operation of homing procedure. | Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. |
| W6017 | Motion task target position is out. | This warning appears with W6014. This warning is triggered when you try to trigger a motion task with an absolute target position outside of the selected modulo range (see also AXIS#.MT.CNTL). | Move the absolute target position of the motion task within the modulo range. Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. |
| W6018 | Motion task target position is out of software limits. | Motion Task position has passed a software limit switch. | Review software limit switch configuration and motion task configurations, and remove incompatibilities. |
| W6019 | Invalid bit combination in the motion task controword. | This warning appears with W6014. This warning is triggered when you try to trigger a motion task with an invalid bit combination in the motion task controword (see also AXIS#.MT.CNTL). | Correct the AXIS#.MT.CNTL setting for the specific motion task. Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. |
| W6020 | 1:1 profile cannot be triggered on the fly. | This warning appears with W6014. This warning is triggered when you try to trigger a 1:1 profile table motion task while another motion task is currently running. | 1:1 profile table motion tasks should be started from velocity 0. Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. |
| W6021 | Customer profile table is not initialized. | This warning appears with W6014. This warning is triggered when you try to trigger a motion task that uses a customer profile table for generating the velocity profile and when the selected profile table is empty (see AXIS#.MT.CNTL and MT.TNUM ). | Change the MT.TNUM parameter for this specific motion task to use an initialized profile table. Activation of any new motion or use of AXIS#.CLRFAULTS clears the warning. |
| W6022 | Motion task activation is currently pending. | A motion task tried to execute before the previous task was able to execute. | Review application timing and allow for adequate time for each motion task to activate before requesting a subsequent motion. |
| W6023 | Homing maximum distance exceeded. | Homing maximum distance exceeded. | Review tuning and parameter AXIS#.HOME.MAXDIST. |
| W6024 | Motion task is not initialized. | This warning appears with W6014. This warning is triggered when you try to trigger a non-initialized motion task. | Initialize the motion task before starting the task. Activation of any new motion or use of DRV.CLRFAULTS clears the warning. |
| W6025 | Homing and feedback mismatch | A homing mode is selected which cannot work with the current feedback. For example, homing modes 3, 6, 10 and 11 require the feedback to provide a Z/index pulse and not all feedbacks provide this signal. If the homing move is started then it may run continuously because it is missing a signal from the feedback. | Select a different homing mode or change the feedback being used. |
| W6026 | Current homing mode requires (see AXIS#.HOME.IPEAK) to be set by user. | The homing mode selected requires that AXIS#.HOME.IPEAK is set to non-zero. | Set AXIS#.HOME.IPEAK to a value non-zero. |
| W6027 | Current command saturated. | AXIS#.IL.CMD has exceeded AXIS#.IL.LIMITP or AXIS#.IL.LIMITN . | Increase current limits (AXIS#.IL.LIMITP or AXIS#.IL.LIMITN ) or reduce load by decreasing trajectory acceleration/velocity. |
| W6028 | Gear feedback source is invalid. | The feedback selected as the gearing source is uninitialized or assigned to the same feedback being used as the commutation, velocity, or position feedback source. | Verify (see AXIS#.GEAR.FBSOURCE) is not 0 and does not match the feedback being used for AXIS#.IL/VL/PL.FBSOURCE. |
| W6029 | Gantry Position error higher than warning threshold. | GANTRY.PL.ERR exceeded GANTRY.PL.ERRWTHRESH. | Increase warning threshold, fix mechanical linkage, improve tuning or remove disturbances. |
| W6030 | Target position was overshot due to invalid Motion Task activation. | The drive cannot decelerate from its current speed to reach the end point of the second Motion Task without moving past it. Increase the deceleration rate in the move or trigger the move earlier.
Note: This warning is only generated if AXIS#.FAULT6004.ACTION is set to 4. |
Change Motion Task profile and clear fault with AXIS#.CLRFAULTS . |
| W7000 | Fieldbus communication lost. |
All fieldbus communication was lost. |
Check fieldbus connections (X11/X12), settings and control unit. |
| W7001 | Fieldbus sync frames lost. | The fieldbus lost synchronization. | Check fieldbus connection or the settings of your fieldbus master. |
| W7010 | Telegram selected by keywords larger than telegram of PLC. | (see PROFINET.USEMODULECFG) is set to 0 and the telegram selected by AXIS#.PROFINET.TELEGRAMID/AXIS#.PROFINET.SUPPTELEGRAMID is larger than the telegram configured in the PLC. Cyclic data will be truncated to the length of the PLC’s telegram. | Change PROFINET.USEMODULECONFIG to use the PLC’s telegram in the drive or set AXIS#.PROFINET.TELEGRAMID/ AXIS#.PROFINET.SUPPTELEGRAMID to a smaller telegram or change the PLC configuration to use a larger telegram. |
| W7011 | EtherCAT Rx received before preparing Tx data finished. |
Within one fieldbus cycle, Rx data from the master was received before the drive finished calculating and copying Tx data.
|
Refer to Synchronization for details on how to validate and adjust EtherCAT synchronization settings or deactivate this warning by setting ECAT.ENRXWARN to 0. |
| IRT configured without isochronous mode. | IRT has been enabled without setting isochronous mode when using telegrams 3 or 5 on either axis. | It is recommended to enable isochronous mode in the PROFINET controller when using telegrams 3 or 5 to guarantee synchronization. If isochronous mode cannot be enabled, the warning can be disabled and bypassed by setting PROFINET.ENISOWARNING to 0. | |
| W7014 | EtherNet/IP dynamic map size exceeds assembly size. | Adjustable sized EtherNet/IP assemblies are in use and either the dynamic command or response maps are larger than the assembly sizes. | Either reduce the number of parameters mapped in the command/response maps or increase the size of the adjustable size EtherNet/IP assemblies being used by the PLC. See Dynamic Assemblies. |
| W7015 | Fieldbus velocity command too low. | Fieldbus commanded a velocity lower than the minimum limit.
Note: This warning is only generated if AXIS#.FAULT7015.ACTION is set to 4. |
Increase fieldbus velocity command. Velocity is clamped at AXIS#.VL.LIMITN. |
| W7016 | Fieldbus velocity command too high. | Fieldbus commanded a velocity higher than the maximum limit.
Note: This warning is only generated if AXIS#.FAULT7016.ACTION is set to 4. |
Reduce fieldbus velocity command. Velocity is clamped at AXIS#.VL.LIMITP. |
| W7018 | Fieldbus cyclic position command not received in time. | One or more fieldbus position setpoints took too long to arrive. If this occurs three or more times in a row, it will trigger F7019. Note: This warning is latched until the drive stops following controller position. | Configure timing properly on the controller side. Ensure the drive and controller clocks are being synchronized. Verify EIP.PLLMODE is set to 1 (CIP Sync). |
| W9000 | Warning: Safe torque off | Safe torque off function has been triggered. W9000 is only generated if AXIS#.SAFE.STO.REPORTFAULT is 1. | Reapply supply voltage to STO if safe to do so. |
| W9007 | Safe brake parameters inconsistent. | The safe parameters, AXIS#.SAFE.SBC.BRAKE#ATTACHED, indicate a brake is attached, but non-safe brake keywords, AXIS#.MOTOR.BRAKE , BRAKE#.AXIS, do not and drive was enabled. |
From the safety parameter screen in WorkBench under safe brake control (SBC), verify the SBC Brake parameters agree with the drive related parameters that a brake is configured or not.
The keywords AXIS#.MOTOR.BRAKE, BRAKE#.AXIS, and SBC configuration all must agree with each other. For example, if no brake is present AXIS#.MOTOR.BRAKE should be 0 and safe parameters for SBC should indicate ‘Not Configured’. If brake is present, AXIS#.MOTOR.BRAKE should be 1, BRAKE#.AXIS should be assigned to proper axis, and safe parameters for SBC should be set to ‘Configured…’
AXIS#.SAFE.SBC.BRAKE1ATTACHED and AXIS#.SAFE.SBC.BRAKE2ATTACHED can be verified for the currently active safe parameters. |
| W9008 | Warning: Brake Test Time Overflow | A safe brake test has not been executed within the configured time limit. | Extend safe brake test time limit or execute a safe brake test. |
| W9009 | Warning: SMM Over Temperature | Safe motion module is over temperature. | Replace hardware. |
| W9010 | Warning: SMM State not operational | Safe motion module is not ready to enable. | Verify safe ID and safe parameters are validated and correct. Check for other faults on the safe motion monitor. |
| W9011 | SMM I/O failure detected. | SMM I/O failure detected. | Update to latest firmware. If problems persist, contact Customer Support. |
| W9012 | Safe brake test cannot start. | Pre-conditions are not met. | Prepare the axis for a safe brake test. Axis must not be faulted, enabled, and at a standstill. All attached brakes must be released. |
| W9013 | Safety rotary switch value differs from validated safe ID. | The rotary switches were changed after the drive completed start-up. | Change the rotary switch value to match the validated safe ID or reboot the drive to validate a new safe ID. |
| W9014 | Developer SMM firmware version detected. | A developer firmware image is on the SMM board. | Load official release firmware. |
| W9015 | Non-certified SMM-drive firmware version pair detected | The SMM and drive firmware images were not certified to function properly together. | Load SMM and drive firmware that have been certified together. Currently, there are only two certified version pairs:
|
| W9016 | Mismatch in drive and SMM safety parameter version | The safety parameter version used at drive startup doesn't match the SMM firmware version. | Reboot the drive. If problem persists, contact Customer Support. |
Related Topics
CANopen Error Codes